TPS60150 Load Regulation

Q: TPS60150 Load Regulation by 1205403

Team,

TPS60150 and has one question regarding the load regulation.

On page 2 in the datasheet is mentioned an output voltage variation of Vout=4.8 to 5.2V. Does this also includes the maximum load regulation ?

Regards,

Matthias


A: Re: TPS60150 Load Regulation by 8433

For Iskip < Iout < 50mA and 2.7V < Vin < 5.5V, Vout remains between 4.8V and 5.2V.  For Iskip < Iout < 120mA and 3.1V < Vin < 5.5V, Vout remains between 4.8V and 5.2V.  When in skip mode (a loads below Iskip), the output could reach 5.3V.  The Iskip threshold has not been characterized but is typically below 1mA.  The IC will provide up to 140mA but the output may droop below 4.8V.


A: Re: TPS60150 Load Regulation by 8433

Yes.