TPS61130 - LBI hysteresis

Q: TPS61130 - LBI hysteresis by 746101

Hi,

is it possible to use the TPS62110's 'adding hysteresis to the LBI input' application note in order to increase TPS61130's LBI hysteresis?

Thanks.


A: Re: TPS61130 - LBI hysteresis by 1090425

Yes.  The LBO/LBI circuit on both is simply a comparator with an open drain output.  Hysteresis can be added with a resistor from the output back to the input.