Welcome to the Non-Isolated DC/DC Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: tps61200 - increased output power by 1184362
Is it possible to increase the output power of the tps61200 using external components?
A: Re: tps61200 - increased output power by 1090425
The TPS61200 uses an average current mode control architecture which limits the average current in the sync FET. It is not peak current limit as in most ICs, so increasing the inductor value to decrease the ripple current will have a minimal effect on the current limit. The current limit cannot be changed with external components.