Welcome to the Non-Isolated DC/DC Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".
Q: TPS61220 Minimum Output Voltage by 1879511
Can the TPS61220 be used for output voltage = 1.2V?
The specs mention 1.8V vout min, while the FB voltage is 0.5V and Vin Min is 0.7V.
Can Vout be 1.2V? What is the limitation?
Regards,
Denislav
A: Re: TPS61220 Minimum Output Voltage by 10449
The TPS61220 can not be used for a 1.2V output. You can not violate the TPS61220 minimum output voltage specification of 1.8V. The output voltage is used to power some of the internal circuitry and must be >1.8V.