TPS61325 - INDLED (O) pin termination when not used

Q: TPS61325 - INDLED (O) pin termination when not used by 145034

What do I do with the TPS61325 INDLED pin if I do not use it?

INDLED ; Output : This pin provides a constant current source to drive low VF LEDs. Connect to LED anode


A: Re: TPS61325 - INDLED (O) pin termination when not used by 244698

 The INLED pin can be left floating if it is not used

Bill Johns