TPS62110 Temperature of device restart

Q: TPS62110 Temperature of device of restart by 667563

 

In the TPS62110 data sheet, it is described clearly that a thermal sensor works at 145 C.

The operating of the device stops when the sensor works.

 

How many degrees is the temperature that the device begins operating again?

 
A: Re: TPS62110 Temperature of device of restart by 1090425

There is a hysteresis temperature of typically 10 degrees C.  So, it will restart at about 135 C.