TPS62122 Output Voltage Range

Q: TPS62122 Output Voltage Range by 3276

Is there anything limiting the 75mA buck converter (TPS62122) from running with an output of about 8V?  The datasheet has it limited to 5.5V.I have one running near 8V and it seems to work okay but I want to know if there are any issues. 


A: Re: TPS62122 Output Voltage Range by 1090425

Yes, the DCS-Control topology requires structures in the IC that are only rated for 5.5V operation.  Operation at 8V is not allowed.

This also applies to the TPS62120.