Q: TPS62230 mode pin by 1158565

Can I use TPS6223x in force PWM mode and control the mode pin by the same signal of EN control. Are there any problems?


A: Re: TPS62230 mode pin by 10449

Yes, you can connect the MODE pin to the EN pin to force the TPS62230 into forced PWM mode operation.  The Electrical CharacteristicsTable shows that both signal have the same electrical requirements to detect a logic high or logic low.