Hi:
I am trying to disable/enable the DCDC1/2/3 and LDO1/2 individually. But I realize that when I disable the LDO2, the DCDC1 and DCDC2 are also disabled.
After I played with CON_CTRL register, I found out that DCDC_SQ2/1/0 affect this behavior.
If I set DCDC_SQ = 111, then disable LDO2 will also disable DCDC1/2. But I can disable DCDC1 without affecting LDO2
If I set DCDC_SQ = 101, then I can disable them individually.
From spec, DCDC_SQ should only affect the power up sequencing. Why does it also affect the individual channel on/off?
Is this a known issue? Is there any side effect if I set DCDC_SQ to 101?
Hongtao