Dear Specialist
Although TPS650250 datasheet describe about typ value of tss (soft start ramp time) , could you provide max value of tss ?
Best regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alpha,
Sorry, we do not spec a min or max Tss time. I have no data to offer you for an estimation either.
What is the main concern for the max Tss spec? If you need to a guaranteed delay then you can use a delay enable circuit if this is the concern you have?
Dear Michael
Could you take a simulation data of Tss?
Our customer has concerned whether TPS650250 can use as VDD of TLK110.
Because TLK110 require VDD rise time is up to a couple milliseconds.
Are there any concern as above?
Best regards.
Hi Alpha,
Why is the TLK110 requiring milliseconds ramp time of VDD? I don't see that specified in the datasheet.
HI
Please see link to this question answered by the TLK team. I see no issue here.
http://e2e.ti.com/support/interface/ethernet/f/903/t/353553.aspx
Hi
Max ramp up time is not guaranteed. It can depend on the Cout and loading specific to only the customers application. The typical number is in reference to the typical use case or application with the recommend Cout and such.
I recommend the customer try their loading and Cout on an evm. Otherwise, if they use the same typical application recommendations then I don't expect a dramatic increase in ramp up time. This however, assumes that they enable the DCDC with a valid VIN already present and able to supply the DCDC demands.
Our customer would like to make sure that TPS650250 startup time is not more than 2,3ms at customer condition.
> It can depend on the Cout and loading specific to only the customers application.
Regarding as above , customer condition is Cout : 95uF and power consumption is 55mA at powerup.
> This however, assumes that they enable the DCDC with a valid VIN already present and able to supply the DCDC demands
Customer has confirmed what you mentioned.
In the condition as above , does customer need to concern about more than 2ms startup time?
Best regards.
Hi,
Thank you providing specific conditions. We can test this in the lab to get a feeling for it but, there will still not be any guarantee to the spec.
Will this do?
Dear Michael
Our customer said if you can provide test data , it is very useful for them.
Could you please test this in your lab?
Customer operation condition is as follow.
Output : VDCDC1
Voltage : 3.3V fixed
Cout : 95uF
Power consumption(at power up) : 55mA
Our customer also need datas including variation cause of lot and temperature.
Best regards.