Hi all,
I am currently attempting to use the AD_IN1-4 pins as a AD converter to detect if a voltage from a seperate device is present. It seems that when I use the AD converter, by setting the TSCMODE register to 110 (A/D measurements) or 111 (TSC and ADC disabled) followed by writing ADCONFIG register with 11010000 (Start AD converstion for AD_IN1 with reference voltage). It seems that when I write to the ADCONFIG register the TSCMODE register changes to usually TSC x-position. This applies the TSREF to AD_IN1, which is undesirable. What way can I use the TPS65072 ADC without the TSC completely disabled?