Hi,
I am using TPS65217D to power my MPU and other peripheral device in the board. The device is powered from USB and we observed that during boot up and during the Wifi enabling the current is shooting beyond 500mA(reaching 600 mA for 2-3 seconds). So i am planning to connect a super cap to the battery pin to supply the deficient current during the peak time. Is it feasible to connect super cap to battery pins of the PMIC? What should the maximum value of super that i can connect? What are the other precautions i should take while connecting the super cap to battery pins.
Regards
Charles