I am using TPS65217C on my board and I have used the Beagle bone black as my reference. I have connected a 5V supply to AC pin of the PMIC. The voltage across SYS1 & SYS2 pins is 0.999V when the voltage is isolated from rest of the board including PMIC via a 0 ohm resistor. I have checked the input voltage rising edge time and it is below 50ms. Could you suggest some tests to figure out if the IC is working fine or needs to be replaced.
I have check the Nreset pin status and PB_In pin status. both are high and show a voltage level of 3.6V.