Hi,
we have designed a Sitara processor based board which is powered by TPS65217C IC.
All the on board voltages for DDR, Processor and other devices are generated using TPS65217C IC.
Couple of months boards worked fine, now we are observing SYS_5V (out put from TPS65217) is falling down to 1.1V instead of 5V,
As SYS_5V is used internally to generate all the remaining voltages , we are not getting any of the out put voltages from TPS65217C.
When I measured the voltages we found CORE and 3V3 voltages are shorted to GND.
Same thing happened with second board also, for this board only 3V3 voltage is showing short, SYS_5V is again dropped to 1.1V.
We have done all the possible passives removal like all decaps, resistors, dry solder effects etc which was not helped to remove the shots,
As per the discussion we had, you will be having idea about the problem we are facing, pls inform if you need any further information on this, Our both working boards are not usable right now because of this problem, our software team is looking for the boards,
We are powering the board using external 5V through Adaptor.
Your quick ideas in resolving this problem will be a great help.
Rgds,
Uma Mahesh