Dear Sir
We can't find NCP18W103J03RC datasheet(TPS65735 EVB suggest part).
May you suggest NTC part for us?
Best Regards,
Bogey
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir
We can't find NCP18W103J03RC datasheet(TPS65735 EVB suggest part).
May you suggest NTC part for us?
Best Regards,
Bogey
Hi Chen,
To get the same results from the datasheet you should select a thermistor with the same B (25/85) value and nominal resistance as the one shown in the specification. R = 10k and B = 3490.
But, to design for different temperature cold and hot trip points you can select another thermistor with a different B value.
Vts = Rt ( at temp) * ITSBIAS.
Vcold and Vhot comparator threshold voltages are specified in the datasheet.
Dear Sir
May we know the TS pin function?
For example, if the Vts > Vcold(2100mV) or Vts < Vhot (300mV), that TPS65735 will action. Is the IC will shutdown or charge function disable?
and from DS page 11, if we use "10K, B=3490 resistor", then we monitor temperature point is 0 degree and 50 degree?
Best regards,
Bogey
HI ,
Typically, when the TS detects the battery to be too hot or too cold the charger disables or reduces the current. I see the datasheet does not specify which one it does. But, since there is only one hot threshold and cold threshold the charger most likely disables charging completely. If you are concerned you can test it out on the EVM that is available on the website
Dear Sir
We have use EVB to test, but EVB will auto into sleep mode(we have try 2 pcs EVB) after EVB run 3X seconds ~ some minutes(random).
set up way as below:
CHG_ON = on
SLEEP = LOW(we also have set to high but result is the same)
VLDO_SET = 3.0V
SW_SEL = S1
Best regards,
Bogey
Hi Chen,
See the user guide to power up the board. It will walk you through the turn on sequence and all jumper options for the EVM. Monitor BAT and provide BAT with a source meter set to 3V allow the current to swing positive or negative.