Are there any maximum inrush current expectation for the TPS65070? I am experiencing an occasional power up problem with this PMIC and am suspecting that it may be caused be excessive inrush current on the AC pin (the inrush appears to exceed 1A at power up). There is no voltage applied to USB or BAT in my application.
When I observe the power up problem, I observe the output of the VDCDC2 to be at the voltage defined by the voltage divider at the DEFDCDC2 pin which is sourced by SYS (the divider resistors are 4.7kohm each). When the PMIC powers up without problems and the OMAP processor boots, the VDCDC2 measures about 3.3V. POWER_ON and PGOOD are logic low when I have the power up problem. PB_OUT is about the same voltage as VDCDC2.
Given this, here are some questions to try and understand the power up problem:
*Is the PMIC possibly in low power mode or an odd state?
*What is causing the PGOOD and POWER_ON to be low?
*Is the OMAP expected to function and drive the POWER_ON high, even when it is only supplied by the ~2.3V to 2.7V I/O level?
*If there are inrush current expectations of the TPS65070 is there a way to set for that or adjust for it?
*When there is a power up problem and I have to manually drive the PB_IN low, does that provide a hint to where my problem lies?