Hi,
Could you advice for the value of external compensation components (Rc, Cc, Cb) for TPS65261. The specification is as below:
1) Vin = 11V ~ 17V (rated at 14V).
2) Vout1,Iout1 = 6V,1.8A
3) Switching Frequency = 1.92MHz
4) Phase margin = 50 ~ 80 degree
5) Gain margin = 20 ~ 40 dB
Reason for asking is because I couldn’t simulate those values in WEBENCH due to the maximum vout is only 5.5V
Thanks