Originally using TPS659113. Now see it is NRND and recommend using TPS6591133. What is different between these two parts and why did TI recommend the change?
On TPS6591133 – pin D7 VBACKUP – what do you do with this pin if you are not using the function?
SWCU083 page 3 says connect it to VCC7 if not used.
Customer design currently has a 2K resistor to GND on VBACKUP pin and they want to change to 1.7K resistor to GND for part commonality. Is this OK?