We are powering on AM3352 with Power Management IC (PMIC). We are having trouble in choosing the PMIC.
We have short-listed TPS65910A3 and TPS650250. We have few questions regarding the IC
- Do we have to use external EEPROM if we are going ahead with TPS65910A3? If yes, how do we code it ?
- How to set the register values in TPS65910A3 ?
- In the datasheet of TPS650250, it is mentioned that the IC is used for Samsung based ARM processors in the Application section. Can we use it to power on AM3352 ?
- Can we use 5Vdc supply as input to TPS650250 instead of battery ?