Dear TI Engineers,
I have customers requesting TPS65023RSB power dissipation value.
Please provide documentation.
Thank you
Hung Truong
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI Engineers,
I have customers requesting TPS65023RSB power dissipation value.
Please provide documentation.
Thank you
Hung Truong
Hi Hung,
The thermal dissipation table is included in the datasheet on page 2.
If you are looking for dissipated power in the device then please use the efficiency curves for the DCDCs on page 14 & 15. Back calculate the Ploss by using the Ploss = Pin - Pout where: Pout = Vout x Iout and Pin = Vin x Iin.
Iin = (Vout x Iout) / (Vin x n) where: n is the expected efficiency at that Vin, Vout, & Iout conditions.
LDO Ploss can be calculated simply by Ploss = Iout x (Vin - Vout)
Read efficiency off the graph for an estimation. Example: using figure 1 in the datasheet:
For:
Iin = Vout * Iout / Vin / n = 1.2V * 10mA / 3.6V / 0.85 = 3.9mA
Ploss = Pin - Pout = Vin * Iin - Vout * Iout = 3.6V * 3.9mA - 1.2V * 10mA = 2.04mW
Hung,
Are you trying to find the dissipation inside the IC package for a thermal analysis or the Ploss of the entire converter including inductor and such?
If you are looking for the entire converter then you can use the method that I described above but, if you are looking for the power loss inside the IC package then that is a bit trickier. You will need to calculate the conduction and switching, (including gate drive and body diode), losses. This app note show a walk through of the calculation that you might be interested in conducting: http://www.ti.com/lit/an/slpa009a/slpa009a.pdf?keyMatch=power%20loss%20buck&tisearch=Search-EN-TechDocs
Since, we don't offer some of the information on the DCDCs of the TPS65023 needed for the calculations described in the app note, I would suggest generalizing and estimating when possible to reduce the calculation head ache. Since, the only major Ploss device outside of the IC is the inductor try using the efficiency curves to estimate total Ploss of the converter and then subtract the inductor ACR, core and DCR losses from the total to get an estimated IC power loss.
See app note from Coilcraft: http://www.coilcraft.com/pdfs/doc486_InductorLosses.pdf
and inductor calculator that combines ACR and core losses: http://www.coilcraft.com/apps/loss/loss_1.cfm?family=xfl3010