Hi,
Customer is using TPS68470/GPIO5 as camera reset signal. The voltage level of this signal is 1.2V. I didn’t see any external pull-up on this signal, and assume it should be configured as a push-pull signal. But I don’t know why it’s 1.2V. I found they add a pull-down resistor (R4620=100kohm) to GND on this signal, is this related to the 1.2V voltage level? Do they need to add this pull-down resistor? WHat shpuld be the expected voltage level here
Thanks!
Antony