Hi,
We specify the absolute rating of LX pins is 6V MAX. Customer now get voltage level(~7V) higher than 6V for short periods. Can you help to confirm if it's ok for us or not?
Thanks!
Antony
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We specify the absolute rating of LX pins is 6V MAX. Customer now get voltage level(~7V) higher than 6V for short periods. Can you help to confirm if it's ok for us or not?
Thanks!
Antony
Antony,
7V has not been tested. Short time it may be OK but long term reliability will suffer. Instead the customer should check the PCB for parasitic inductance on the VIN new for the switcher that sees the high voltage spike and whether there is a way to improve it. Since we know that this violates the PDK I would say that this is NOT OK. It may work but we can't guarantee it.
Chase
Hi,
Additional to the LX spike voltage concern, customer also find jiter issue for buck5 (around 42% @ 5A load). What can they do to improve this from either their schemaitcs, layout or PMIC registers?
THanks!
Antony
Hi
Additional to the LX spike voltage concern, customer also find jiter issue for buck5 (around 42% @ 5A load). What can they do to improve this from either their schemaitcs, layout or PMIC registers?
They’re using 5V as system input instead of 1S battery. I’m not sure if it matters.
Addititonally, they also find poor jitter performance on Intel board using our chip.
Please see jitter plot and layout plot as attached and provide your comments what they can do to improve these.
Test Point |
BUCK5 LX1 |
BUCK5 LX2 |
||||||
0A |
0.23A |
2.5A |
5A |
0A |
0.9A |
2.5A |
5A |
|
Intel board(+VSYS=+3.7V) |
4.87% |
12.80% |
38.70% |
>100% |
|
8.40% |
36.90% |
32% |
Redmond(+VSYS=+5V) |
5.90% |
14.37% |
57.80% |
>100% |
|
10.91% |
9.95% |
46.47% |
Redmond(+VSYS=+3.7V) |
4.59% |
13.37% |
57.14% |
>100% |
|
8.71% |
7.49% |
36.30% |