Hello、
I use TPS65185 for EPD.
I have question about VSET( 0x02h )register and set value.
VSET[2:0] can set "011 - ±15.000 V" to "110 - ±14.250 V". These value written in datasheet page 30.
However, VDDH_OUT and VEE_OUT parameter in operating condition datasheet page 8 seems be able to set over voltage.
The test condition of VDDH_OUT parameter VSET = 22V and the test condition of VEE_OUT parameter VSET = -20V.
These are also written in page 8.
VSET[2:0] register can be set +22V and -20V only in test conditions?
Would you please let me know this inconsistency?
Best Regards, Nobuyuki Hayama.