Hello,
We wired the LM26484 as described in the datasheet "Typical Application" diagram, and it is not working correctly. We are noticing that it is pulling 1.7A and getting very hot. What could be the issue?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
We wired the LM26484 as described in the datasheet "Typical Application" diagram, and it is not working correctly. We are noticing that it is pulling 1.7A and getting very hot. What could be the issue?
Sheng,
The device was enabled and the voltage was 3.8V at the Buck outputs.There are no shorts--thess outputs go directly to a header to power a peripheral device (which was not connected).
I've removed the device from our circuit, and the short circuit condition has been removed.
Hi,
I got the schematic from our CAT group for this customer/issue, seems there is an error at LDO output, the FB pin doesn't connect to the output.