We are trying to debug issues on Gumstix board which uses the TWL6030 for its power management and also RTC.
I contacted out local Ti Distributor to get the TWL6030 datasheets but no answer from them as to how to get the datasheet.
We are in Perth Western Australia
How do we get the NDA so we can get the datasheet and debug the configuration to determine an issue with the RTC dropping the time by indicating POR despite the RTC Battery being at suitable voltage (2.6V). There is insufficient information in the general documentation on the TWL6030 page and no indication how we get the data, only on post on a read only forum which is someone else asking how to get the register map.
Need to see if the Linux kernel is correctly configuring the RTC as we shouldn't be losing the clock but are and we need to retain the clock!
Help please!