This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6590377 GPIO and I2C addresses

Hi,

I am using the TPS6590377 PMIC device in my design. I had some confusion regarding a few connections and the I2C addresses. I have listed them below.

1. GPIO: In our design, the GPIOs 0 to 7 are all unused. When GPIO_1 and GPIO_4 are unconnected, the datasheet recommends them to be left floating, whereas as per the design guide they should be connected to ground. Please tell me the recommended connection for all the GPIO pins 0 to 7 when unused.


2. I2C addresses: As per the page 8 of the PMIC user guide, the I2C1 addresses are 0x58, 0x59, 0x5A & 0x5B. However, as per the datasheet, the addresses are 0x48, 0x49, 0x4A & 0x4B. Which addresses should be referred to?

3. REGEN1: There is a confusion regarding the level of this signal. The user guide shows this as 1.8V signal - page12.
As per PMIC datasheet, this signal is in VCC1 (3.3V) domain. Please let me know the correct voltahe level.
Also, in the AM572x General Purpose EVM Processor Module, this pin has a pull up to 3.3V. As per my understanding, this pin is active high and should have a pull down to ground, so that the subsequent supply is enabled when it is asserted. Can you please explan me why this pull up is provided in the EVM?

Thanks and Regards,
Prachi