Hi!
I am starting to work with the TI TPS65835 chip and was wondering if there is already CCS support for it. I can't seem to find the support files onthe product's web page, nor is it included by default in my CCS version (6.1.3.00033).
By reading through the forums I saw that at least at one point in time, the TPS65835 support for CCS was planned. I am referring to the following thread in which Mr. Christopher Johnson from TI wrote about the planned support (the post is quite old so i decided to open a new topic):
I've also looked at an example code for the mentioned chip from the following post and also found a "TPS65835.h" header file, which seems to be missing in the default CCS installation:
I would appreciate any input on whether the TPS65835 is supported in CCS and if so, where can I find the install package mentioned in the first linked post.
If working on the support package was canceled and none exists, I would appreciate guidance on how to approach developing code without it. Do i work with the msp430g2553 MCU as the target device when making a new CCS project and use the msp430g2553.h header file?
Thank you in advance for all your help.
Cheers!