• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Power Management » PMU » PMU Forum » TPS65251
Share
PMU
  • Forums
  • E2E Wiki
Options
  • Subscribe via RSS

TPS65251

TPS65251

This question is answered
Ignacio Linares
Posted by Ignacio Linares
on Jun 10 2010 11:20 AM
Expert1210 points

Questions about the TPS65251 datasheet: 

On Page 13 (Overview) it says, “The device has two built-in LDO regulators. During a standby mode, the 3.3-V LDO and the 6.5-V LDO can be

used to drive MCU and other active loads.”

How much current can these LDO’s source to external loads? The electrical Characteristics table on page 6 specifies the output voltages, but not the currents.

 

Also, the datasheet doesn’t contain any information about power down. I assume from this that when a converter is “shutdown” due to either an over-current or UVLO condition, the high side FET is shut-off, and the output voltage is simply allowed to decay through the load. But, what is done with the low side FET? Is it turned-on or off? I’m not sure if this really matters, but I worry about oscillation if it is turned-on during shut-down and the load is too light to damp the resulting tank circuit formed by the output inductor and capacitors. This could also be an issue if I back feed the 1.8 V rail from the 3.3 V rail during shutdown to ensure that 2 V differential is not exceeded (requirement for power sequencing AM1808 per SLVA371A App Note).

 

Per SLVA371A section 1.1, I need to sequence as follows: 1.2V->1.8V->3.3V and ensure 3.3V never exceeds 1.8V by more than 2V (per note 3 section 1.1 of app note).

All that said, I think I can make this part work for me (for powering the AM1808 per SLVA371A) with the following configuration.

  1. Floating the 1.2 V supply enable pin so it starts as soon as 12 V is applied to Vin.
  2. Delay the 1.8 V power-up by placing a cap on its enable pin, so it comes up after the 1.2 V rail.
  3. Connect the 3.3 V enable pin to the 1.8V rail through a voltage divider and place a cap on its soft-start pin to ensure it comes up after the 1.8V rail and is shut-off whenever the 1.8V drops below 1.6-1.5 V.

 

That just leaves ensuring that 3.3 V – 1.8 V is always less than 2 V during power-down. I think I can do that by either engineering the decay rates to maintain that difference under different loading conditions, or by placing a 1.9 V LDO between the 3.3 V and 1.8 V rails.

Any thoughts?

Also,

1.       The datasheet mentions the following on the first page (second paragraph from the bottom):   TPS65251 features a supervisor circuit that monitors each converter output. The PGOOD pin is asserted once sequencing is done, all PG signals are reported and a selectable end of reset time lapses. The polarity of the PGOOD signal is active high.  How does one set the “selectable end of reset time”?. 

2.       What is the threshold voltage for the EN (enable) pin?  I assume it is around 1.3V, but the datasheet doesn’t specify it.

 

 

 

TPS65251 AM1808 SLVA371A OMAP-L138
Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Ignacio Linares
    Posted by Ignacio Linares
    on Jun 10 2010 18:38 PM
    Expert1210 points

    I found the threshold voltage for the EN pin in the datasheet.  It is Vil=1.24V and Vih=1.55V.

    SLVA371A
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Ignacio Linares
    Posted by Ignacio Linares
    on Jun 14 2010 13:36 PM
    Suggested Answer
    Expert1210 points

    Here the answers:

     

    .       The datasheet mentions the following on the first page (second paragraph from the bottom):   TPS65251 features a supervisor circuit that monitors each converter output. The PGOOD pin is asserted once sequencing is done, all PG signals are reported and a selectable end of reset time lapses. The polarity of the PGOOD signal is active high.  How does one set the “selectable end of reset time”?.  It is not covered in the datasheet.  Jeff would like to use this to hold the processor in reset until the rails are stable.  If one of the rails drops out of regulation, he wants to hold the processor in reset for a minimum period. 

     

    For the catalog part TPS65251 the reset time is 1s (fixed) after all rails are powered up and the PG flag (internal) is asserted.

     

    2.       What is the threshold voltage for the EN (enable) pin?  I assume it is around 1.3V, but the datasheet doesn’t specify it

     

    From latest spec

     

    .

     

    3.       What is the availability of the device?  TI website shows it as Active and samples can be requested.

     

    RTM process is on-going, pedro can update you on this.  Samples and EVMs can be supplied directly from our group.

     

    On Page 13 (Overview) it says, “The device has two built-in LDO regulators. During a standby mode, the 3.3-V LDO and the 6.5-V LDO can be

    used to drive MCU and other active loads.”

    How much current can these LDO’s source to external loads? The electrical Characteristics table on page 6 specifies the output voltages, but not the currents.

     

    We suggest not to go beyond 10mA (see attached foils).

     

    Also, as we noted yesterday the datasheet doesn’t contain any information about power down. I assume from this that when a converter is “shutdown” due to either an over-current or UVLO condition, the high side FET is shut-off, and the output voltage is simply allowed to decay through the load. But, what is done with the low side FET? Is it turned-on or off? I’m not sure if this really matters, but I worry about oscillation if it is turned-on during shut-down and the load is too light to damp the resulting tank circuit formed by the output inductor and capacitors. This could also be an issue if I back feed the 1.8 V rail from the 3.3 V rail during shutdown to ensure that 2 V differential is not exceeded.

     

    On power-down both fets are switched-off.  Device relies on feedback chain resistors to discharge output

     

    All that said, I think I can make this part work for me with the following configuration.

    1. Floating the 1.2 V supply enable pin so it starts as soon as 12 V is applied to Vin.

    There is a 10ms delay from the time when Vin UVLO is asserted to the time converter starts

    1. Delay the 1.8 V power-up by placing a cap on its enable pin, so it comes up after the 1.2 V rail.

    OK

    1. Connect the 3.3 V enable pin to the 1.8V rail through a voltage divider and place a cap on its soft-start pin to ensure it comes up after the 1.8V rail and is shut-off whenever the 1.8V drops below 1.6-1.5 V.

     

    That just leaves ensuring that 3.3 V – 1.8 V is always less than 2 V during power-down. I think I can do that by either engineering the decay rates to maintain that difference under different loading conditions, or by placing a 1.9 V LDO between the 3.3 V and 1.8 V rails.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Ignacio Linares
    Posted by Ignacio Linares
    on Jun 14 2010 13:40 PM
    Suggested Answer
    Expert1210 points

    Here the answers:

     

    1.  For the catalog part TPS65251 the reset time is 1s (fixed) after all rails are powered up and the PG flag (internal) is asserted.

     

    2.      Found in latest spec

    3.   RTM process is on-going, pedro can update you on this.  Samples and EVMs can be supplied directly from our group.

     

          4. We suggest not to go beyond 10mA (see attached foils).

     

          5.  On power-down both fets are switched-off.  Device relies on feedback chain resistors to discharge output

     

    All that said, I think I can make this part work for me with the following configuration.

    1. Floating the 1.2 V supply enable pin so it starts as soon as 12 V is applied to Vin. There is a 10ms delay from the time when Vin UVLO is asserted to the time converter starts
    2. Delay the 1.8 V power-up by placing a cap on its enable pin, so it comes up after the 1.2 V rail. OK
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • YG Kim
    Posted by YG Kim
    on Jul 06 2010 19:53 PM
    Intellectual2025 points

    Hello.

    1.We recommend 3.3V and 6.5V LDO external current 10mA.

    2.Power down: all enable pin goes to GND and all three bucks no operation.

    3.Over current and short circuit: The parts goes to hiccup-mode operation meaning is that high side and low side switching.

    4.Power sequecny : Delayed start-up, see TPS65250 data sheet page 18,

    5.PG GOOD reset timer: set defauit PG timer 1000msec but if you need select one of those power good timer too but need change EEPROM, 32msec,256msec and 2sec.

    6. Enable threshold votage is 1.55V - 1.3V.

     I am not sure, the above answer is enough or not, any more question, please send e-mail to me, yg_kim@ti.com

    Regards YG Kim

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • YG Kim
    Posted by YG Kim
    on Jul 20 2010 12:37 PM
    Verified Answer
    Verified by Ignacio Linares
    Intellectual2025 points

    see above my comments. YG

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use