Dear all.
Do you have VOL parameter of PGOOD?
Pull up : 100K ohm (EVM) or 10K (customer board)
VCC : 3.3V
Regards,
PAN-M
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all.
Do you have VOL parameter of PGOOD?
Pull up : 100K ohm (EVM) or 10K (customer board)
VCC : 3.3V
Regards,
PAN-M
VOL means low level output voltage capabirity.
ex. When VCC=5V and IOL=4mA, VOL(typ)=0.25V VOL(max)=0.4V.
Do you have VOL parameter of PGOOD.
Regards,
PAN-M
hi,
for TPS65251 PGOOD VOL:
When Vin=12V and IOL=3mA, VOL(typ)=0.245V VOL(max)=0.28V
thanks.