We have an existing design with many units in the field operating correctly with the TPS65217A supply. I am doing a failure analysis of one returned unit where the supply has the wrong output voltages before quickly shutting down, about 30% higher than expected. The INT_LDO and BYPASS pins also have proportionally higher voltages.
I have replaced the IC 3 times with the same result, so it is not a failure of the IC itself. Any idea what external components or PCB defect could cause this symptom?