I was reviewing the SLVU731A application note on how to power the AM335x family of processors using the TPS650250. It is noted that the part has support for DDR3 when properly configuring the DCDC2 step down converter. However, I still had a few questions regarding the sequencing. Are the LDO's 1.8V rails capable of being run off the DCDC3 3.3V rail and still meet the sequencing requirements for the AM335x with DDR3?