Hi Team,
can you help to provide the threshold voltage of VSx in TPS650832? Thanks!
threshold voltage in TPS650832 | |
VSA | |
VSB | |
VSC | |
VSD | |
VSE | |
VSF | |
VSG | |
VSH |
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
can you help to provide the threshold voltage of VSx in TPS650832? Thanks!
threshold voltage in TPS650832 | |
VSA | |
VSB | |
VSC | |
VSD | |
VSE | |
VSF | |
VSG | |
VSH |
Marvin,
These values are defined in the datasheet Table 6-1 in the 3rd column "Comparator Input". There it states the voltage and whether it is a logic input or an analog input. If it is an analog input the voltage defined in this table +/- 5% is the threshold for output going HIGH depending on the direction of the voltage change.
Threshold is +/-8% for output going LOW. Thus, there is 3% hysteresis on the +/-5% threshold value from the defined voltage in the table 6-1. See page 19 for threshold values.
If the table says "Logic Input" then the comparator is TTL logic, thresholds are defined in electrical specs on page 18.