Hi All,
We are working with TI-DM3725 and TPS69590 and facing issue in sending the device to low power mode and resuming from it.
With the tps69590, low power mode couldn't be achieved properly by clearing the FUNC_CTRL[6].SUSPENDM bit.
When clearing this SUSPENDM bit, ports are getting disabled (i.e., device disabled from device manager) and can see power drop of 40mA in power supply.
but could not resume exiting the low power mode.
When re-plugged the device, device is appearing as "Unknown device recognized".
We have configured the tps unit as per the tech reference manual, didn't find anything specially to be configured for low power mode. if there is anything needs to be taken care, please let me know.
Also I didn't find any relevant errata workaround for this issue.
Have anyone faced this problem before and if yes, could you please suggest us the
workaround for it.