This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65910A3EVM-583: nRESPWRON

Part Number: TPS65910A3EVM-583

HI ,

We are using TPS65910A3 as the PMIC for our AM335X based Board .

The PMIC is having a pin "nRESPWRON " . I am having a bit of a confusion with the pin .
It is suggested to connect this pin to the "PWRONRSTn" of the controller .

This is what i understand :

When we power the board , initially the "nRESPWRON " will be low keeping the AM335X in reset and once the power sequencing is over , it will be high releasing the AM335X from reset and boot up normally .

Correct me if I am wrong 

Regards 
Eby Jayan