Hi,
We have a product that we use on vehicles. We intend to use the TPS65320C with our new design. We need to reduce the voltage from the car battery to 4.4V and 3.3V. There's a car battery on the Buck input(Vin pin). We want to get 4.4V at the buck regulator output. We feed LDO input with Buck output and we want to get 3.3V at the LDO regulator output.
We produced our test card and soldered the power circuit. When the input is between 7V and 11V, we can get the desired voltage(4.4V) at buck regulator output,but buck regulator output is increasing with input voltage while input is above 11V. When the input is 26V, the output goes up to 11V and is not stable. With that there is no problem at the LDO regulator output there we are getting 3.3V. But buck regulator does not work stable. We have not encountered any errors in the schematic and the PCB.
Could it cause trouble, can you help?