Other Parts Discussed in Thread: OMAP-L138,
I'm using TPS65070 for a new redesign that powers OMAP-L138 and Cyclone 4 FPGA. The present design uses 5.4V input to the PMIC. For my new design, I'd prefer to boost this voltage to 6.3V. From the 65070 datasheet, the AC input max is 5.8V, but the VINDCDC input max is 6.3V. I understand this is due to the overvoltage protection built into the power path controller. I don't need or use the USB or BAT inputs (they have a capacitor to ground).
So can I bypass the power path controller, and feed 6.3V directly into VINDCDC(1,2,3)?
If so, what do I do with the various power path pins?
Thank you!
David