I have a customer who is asking the following question:
What is the behavior and reaction time of the PPATH input when the Vsys load exceeds the PPATH current setting for the TPS65217?
Example - 5V AC power is applied, battery and USB power is NOT applied, the IC completes the power up sequence, IAC is set to "01" (the 500mA limit) and later Vsys is shorted to PGND (or exceeds the 580mA max limit by 1mA for a 1us). Does the AC input disconnect from the Vsys pin and if so how quickly?
Is the behavior the same for the USB input (no other power input applied)? For the Battery input (no other input power applied)?
Thanks for your help with this questions.
Richard Elmquist