I am designing an application that will run off a car battery. In the event the car battery voltage is removed my system will run off an emergency battery just long enough to shut down gracefully. I noticed that when I unplugged incoming voltage that the VDDCTRL died as well. After looking at the datasheet I see that V5IN must have more than 4.5V on it. This means that I will not be able to run this off a single cell 4.2V LiPO battery.
Is there a way to run VDDCTRL down to 3.5V or am I going to have to design in a boost regulator?