Hi,
We got a question from customer about TPS43350-Q1.
Could you help us?
[Question]
If the IC exceeds the maximum duty 98.75%, how is the behavior of the IC?
- condition -
Vin=8V to 16V
Vout=8V
fsw=400kHz *synchronized to external clock
They want non pulse skip operation, even if the output voltage falls. Does the IC meet to their requirement?
Best Regards,
tateo