Hello!
I have a schematic based on TPS650830 as PMIC and external VRM powering Kaby Lake and I have and EC that is powered from VR3 3.3V (ENVR3 is driven by LDO3V). The situation is so, that I need all Kaby Lake power to be turned off except VR3).
The questions are:
1) If EC for example will bring SHUTDOWNZ low - VR3 will be also turned off?
2) In shutdown mode power button events are still processed and PCH_PWRBTNZ, EC_ONOFFZ outputs are working?
3) If there any HW way (not using SMB access) to turn off all power outputs except VR3 (one way is to drive all ENVRx from logic & (SLP_x lines & EC shutdown line))?
Thanks in advance.