Hi
I followed the VAYU EVM to develop our customer board.
I use RESET_IN of PMIC to control power ON/OFF event.
Other control signals are floating include PWRON, RPWRON, PWRDOWN as VAYU EVM.
The VDDA_RTC of PMIC is only 1.1V when CPU can't power on.
I have checked the 3.3V, 5V is OK and RESET_IN release after 3.3V, 5V power up around 5mS.
The power on fail is not always that the fail rate about 1/3.
Are any signals must to check with power on fail?
thank you.