Other Parts Discussed in Thread: AM4378
Hi,
I recieved one PCN recently. It is for revision up data sheet of TPS65218 rom B to C.
According to the Revision history of data sheet, many items are changed.
For example,
In Figure 1-1. Simplified Schematic,
INT_LDO pin's capacitor value is changed from 100nF to 1uF.
L5 pin's inductor value is changed from 10uH to 1.5uH.
SDA/SCL pin's resistor value are changed from 4.7k ohm to 100k ohm.
Also, DCDCx output voltage range are changed.
My customer uses TPS65218 with AM4378. Their design is based on AM437x StarterKit. But they had refered older data sheet (rev.B) of TPS65218 for their board design.
So I am afraid AM4378 may not work with new TPS65218 spec(I 'don't know TPS65218 has new silicon or not). Is this new data sheet of TPS65218 no effect to older AM4378 board design?
Please advise me.
Best regards,
Michi