Default, when VDD1 UV(Under Voltage) / OV (Over Voltage) happens, VMON of TPS65381A-Q1 will detect this condition , but will not let ENDRV going to LOW status, because NMASK_VDD1_UV_OV bit is set with 0 by default. and there are no other register's bit used to mask VDD3/5 or VDD5 line for OV / UV condition. Why?
Is there the case, VDD1 will not be used?
VDD1 UV/OV condition is not worth for TPS65381A-Q1 to detected and let ENDRV to LOW by default?