Dear all
Could you give me the advise of TPS65917-Q1 output accuracy?
Our customers are considering using TPS65917-Q1 as the power supply for FPGA Core voltage.
The requirements of the FPGA are as follows
・VCC INT voltage : 0.85V
・Output accuracy:±3%(include load transiant)
The output voltage accuracy of TPS 65917-Q1 is -1%~2%, and the accuracy of Transiant is typ 3%.
Customers are concerned about whether they can realize the 3% required by FPGA.
■Question
Does Transient's accuracy of 3% also include output voltage accuracy?
If it is difficult, would you advise me If you have any other ideas.
Best regards
Masa0301