Other Parts Discussed in Thread: AM3358
It is unclear to me if the 32kHz input on the TPS65910 is required (OSC32KIN/OSC32KOUT). If you don't need the internal real time clock feature then can these pins be left floating? I looked at the schematic checklist for this part and the "Not Used Feature" for these pins is listed at N/A which tells me you can't not use this feature. Can someone please clarify?