In the TPS65916 design checklist it indicates that the above GPIO's have a voltage level of VRTC(1.8V) but are 5.25V tolerant. If I am using these as an input. for example GPIO_1 as RESET_IN, can the input signal be tied to 3.3V or does it need to be 1.8V?
Thanks!