The application report SLVA901 address a fault due to Vin brownout when there is no battery.
Can you go into more detail of what this fault is?
I assume the fault is that PMIC SYS output turns off when a brownout occurs but does not come back up upon Vin recovery.
My circuit is like Case A in SLVA901 and when Vin drops below 3.6 Volts the PMIC turns off and does not turn back on when VIN is returned to 5.0V.
I tried solution circuit number 2 and the same thing still happens. I had assumed that the PMIC would turn back on when the Vin voltage recovered.
Is this because the brownout lasted more than 1 second?