Other Parts Discussed in Thread: TMS570LS1114
Hello,
I am testing the ability of the TPS DIAG_OUT pin. For DMUX everything is fine.
For AMUX I observed that the voltages are not as expected:
Diag_Mux_Sel | Signal Name | Divide Ratio | Divide Acc | V [V] | UV [V] | OV [V] | V [digits] | VUV [digits] | VOV [digits] | Meas [digits] | Measdiv [V] | Meas [V] |
0x01 | VDD5 | 2 | 2,25% | 5,00 | 4,500 | 5,450 | 3102 | 2729 | 3458 | 2653 | 2,137 | 4,27 |
0x02 | VDD6 | 3 | 3,75% | 6,00 | 5,200 | 8,200 | 2482 | 2070 | 3519 | 1715 | 1,382 | 4,15 |
0x04 | VCP | 13,5 | 6,25% | 4,000 | 15,000 | 0 | 345 | 1465 | 819 | 0,660 | 8,91 | |
0x08 | VSOUT1 | 4 | 1,20% | 0,00 | 3,300 | 9,500 | 0 | 1011 | 2983 | 16 | 0,010 | 0,04 |
0x10 | VBAT_SAFING | 10 | 5,50% | 12,00 | 4,200 | 36,700 | 1489 | 493 | 4805 | 475 | 0,380 | 3,80 |
0x20 | VBATP | 10 | 5,50% | 12,00 | 4,200 | 36,700 | 1489 | 493 | 4805 | 475 | 0,383 | 3,83 |
0x40 | MAIN_BG | 1 | 0,00% | 2,49 | 2,364 | 2,617 | 3090 | 2934 | 3247 | 2983 | 2,405 | 2,41 |
0x80 | VMON_BG | 1 | 0,00% | 2,49 | 2,364 | 2,617 | 3090 | 2934 | 3247 | 2963 | 2,388 | 2,39 |
Except MAIN_BG, VMON_BG and VCP all voltages are not in valid ranges. VSOUT1 is not used. I did the measurements ("Meas") with internal ADC of TMS570LS1114 (VRef = 3.3V, 12 bit resolution) as well as with Voltmeter.
The left 7 columns are obtained from the data sheet. "V [Digits]" means expected voltage at DIAG_OUT pin in Digits. "Meas [digits]" means measured voltage at DIAG_OUT pin in digits. "Measdiv [V]" means measured voltage at DIAG_OUT pin in volt. "Meas [V]" means measured voltage with respect to divide ratio in Volt.
The voltages on the output Pins of TPS are all correct (e.g. VDD5 = 5V, VDD6 = 6V,...). Is there a Problem with divide ratio? Because with divide ratio 1 everything is fine.
Greetings Helge