This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65910: VBACKUP Consumption when device is OFF State

Part Number: TPS65910
Other Parts Discussed in Thread: AM3351

I am using the PMIC  TPS65910A31A1 with sitara AM3351. I am using the RTC from the PMIC with the  internal oscillator  and the VBACKUP supply is the battery CR2032(3V).

My case is:

When the device is ON, the current in the VBACKUP pin is 0 A. (correct)

When i put PWRON  in '0' for 8 seconds the  PMIC goes to OFF State. In this state (OFF) the current in VBACKUP pin is 0,35mA, and in the datasheet the number for this situation is  max. 42uA. (Wrong).

The RTC keep the clock, but with this current, the CR2032(168mAh).is valid for only 20 days . When the correct will be at least 160 days.

So, what is wrong with my circuit?

Thanks.