Other Parts Discussed in Thread: PMP12004-HE
Hello,
My question regards the default voltage levels of TPS65086401. It is to be used with a Xilinx Zynq UltraScale Mpsoc+ XCZU5EG. The reference design for TPS65086401 is designed for XCZU9 and XCZU15 which differentiates somewhat from XCZU5. The biggest problem being that for the case with XCZU5 different default voltage levels would be necessary. Is it possible to order TPS65086401 and get Factory OTP Programming for other specified votlages levels. If not, how should one design for use with, for example, DDR4 which requires VPP 2,5 V (not availabe as default voltage output). Can't boot Zynq without DDR and hence not configure TPS65086401 votlage levels over I2C.
And why is the refernce design connected such that VCCINT (PL) etc. is connected to a 3 A buck, when estimations on smaller devices show that the current consumption of these supplies usally goes up quite a bit above this?
B.r. Mattias